SPRUJ27C November 2022 – November 2023 TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1
Initializes the Flash API
Synopsis
Fapi_StatusType Fapi_initializeAPI(
Fapi_FmcRegistersType *poFlashControlRegister,
uint32 u32HclkFrequency)
Parameters
| poFlashControlRegister [in] | Pointer to the Flash Memory Controller Registers' base address. Use F021_CPU0_BASE_ADDRESS. |
| u32HclkFrequency [in] | System clock frequency in MHz |
Description
This function is required to initialize the Flash API before any other Flash API operation is performed. This function must also be called if the System frequency or RWAIT is changed.
Flash control register base address is hard coded in this function internally and does not use the value (first parameter passed to this function) provided by the user. However, if there is a mismatch between the internal hard coded value and the user provided value, a warning is returned to the user even though the initialization steps still take place normally.
Return Value
Sample Implementation
#include “F021_F28003x_C28x.h”
#define CPUCLK_FREQUENCY 120 /* 120 MHz System frequency */
int main(void)
{
//
// Initialize System Control
//
Device_init();
//
// Call Flash Initialization to setup flash waitstates
// This function must reside in RAM
//
Flash_initModule(FLASH0CTRL_BASE, FLASH0ECC_BASE, DEVICE_FLASH_WAITSTATES);
//
// Jump to RAM and call the Flash API functions
//
Example_CallFlashAPI();
}
#pragma CODE_SECTION(Example_CallFlashAPI, ramFuncSection);
void Example_CallFlashAPI(void)
{
Fapi_StatusType oReturnCheck;
//
// This function is required to initialize the Flash API based on
// System frequency before any other Flash API operation can be performed
// Note that the FMC register base address and system frequency are passed as the parameters
//
// This function must also be called whenever System frequency or RWAIT is changed.
//
oReturnCheck = Fapi_initializeAPI(F021_CPU0_BASE_ADDRESS, CPUCLK_FREQUENCY);
if(oReturnCheck != Fapi_Status_Success)
{
Example_Error(oReturnCheck);
}
//
// Fapi_setActiveFlashBank function initializes Flash bank
// and FMC for erase and program operations.
//
oReturnCheck = Fapi_setActiveFlashBank(Fapi_FlashBank0);
if(oReturnCheck != Fapi_Status_Success)
{
Example_Error(oReturnCheck);
}
//
// Erase Program
//
/* User code for further Bank flash operations */
.
.
.
.
//
// Example is done here
//
Example_Done();
}