SPRUJ31 april 2022
The F28003x LaunchPad has several power domains that can be connected or isolated from each other with removable shunts. The different 3.3 V and 5 V power domains are further described in Figure 3-2 and Figure 3-3.
Table 3-1 describes the usage of the different removable shunts on the LaunchPad board.
| Shunt Identifier | Usage Description |
|---|---|
|
JP1, +5V0 |
Connects the +5 V power from the USB-C connector (+5V0_USB) to the +5 V power on the XDS110 side of the board (+5V0_XDS110). Bridges the power and ground isolations between the two board sides. |
|
JP1, GND |
Connects the board Ground on the isolated USB-C connector side of the board (USB_GND) to the rest of the board ground (GND). Bridges the power and ground isolations between the two board sides. |
| JP2, +5V0 | Connects the +5 V power on the XDS110 side of the board (+5V0_XDS110) to the +5 V power on the F280039C side of the board (+5V0_MCU). |
| JP2, +3V3 | Connects the +3.3 V power on the XDS110 side of the board (+3V3_XDS110) to the +3.3 V power on the F280039C side of the board (+3V3_MCU). |