SPRUJF1D November   2024  – April 2026

 

  1.   1
  2.   Description
  3.   Get Started
  4.   Features
  5.   5
  6. 1Evaluation Module Overview
    1. 1.1 Introduction
      1. 1.1.1 Preface: Read This First
        1. 1.1.1.1 Sitara MCU+ Academy
        2. 1.1.1.2 Important Usage Notes
    2. 1.2 Kit Contents
    3. 1.3 Device Information
      1. 1.3.1 System Architecture Overview
      2. 1.3.2 Component Identification
      3. 1.3.3 Functional Block Diagram
      4. 1.3.4 BoosterPacks
      5. 1.3.5 Device Information
        1. 1.3.5.1 Security
  7. 2Hardware
    1. 2.1  Setup
      1. 2.1.1 Standalone Configuration
    2. 2.2  Power Requirements
      1. 2.2.1 Power Input Using USB Type-C Connector
      2. 2.2.2 Power Tree
      3. 2.2.3 Power Status LEDs
    3. 2.3  Header Information
      1. 2.3.1 OSPI Expansion Connector
      2. 2.3.2 ADC/DAC External VREF Headers
      3. 2.3.3 FSI Header
      4. 2.3.4 EQEP Headers
    4. 2.4  Push Buttons
    5. 2.5  Reset
    6. 2.6  Clock
    7. 2.7  Boot Mode Selection
    8. 2.8  GPIO Mapping
    9. 2.9  IO Expander
    10. 2.10 Interfaces
      1. 2.10.1  Memory Interfaces
        1. 2.10.1.1 OSPI
        2. 2.10.1.2 Board ID EEPROM
      2. 2.10.2  Ethernet Interface
        1. 2.10.2.1 Ethernet PHY 0 - RGMII2 / PR0_PRU0
        2. 2.10.2.2 Ethernet PHY 1 - RGMII1 / PR0_PRU1
      3. 2.10.3  I2C
        1. 2.10.3.1 Industrial Application LEDs
      4. 2.10.4  SPI
      5. 2.10.5  UART
      6. 2.10.6  MCAN
      7. 2.10.7  SDFM
      8. 2.10.8  FSI
      9. 2.10.9  JTAG
      10. 2.10.10 Test Automation Pin Mapping
      11. 2.10.11 LIN
      12. 2.10.12 ADC and DAC
      13. 2.10.13 EQEP
      14. 2.10.14 EPWM
      15. 2.10.15 USB
    11. 2.11 BoosterPack Headers
      1. 2.11.1 BoosterPack Mode 00: Standard LaunchPad/BoosterPack Pinout
      2. 2.11.2 BoosterPack Mode 01: Servo Motor Control BoosterPacks Mode
      3. 2.11.3 BoosterPack Mode 10: BOOSTXL-IOLINKM-8 Mode
      4. 2.11.4 BoosterPack Mode 11: C2000 DRVx BoosterPacks Mode
    12. 2.12 Pinmux Mapping
    13. 2.13 Test Points
    14. 2.14 Best Practices
  8. 3Software
  9. 4Hardware Design Files
  10. 5Compliance
  11. 6Additional Information
    1. 6.1 Revision E1 Appendix
      1. 6.1.1 TA_POWERDOWNz pulled up by VSYS_TA_3V3 which is powered by VSYS_3V3
      2. 6.1.2 USB2.0_MUX_SEL0 pulled up by R355
      3. 6.1.3 MDIO and MDC of PRU0-ICSS0 needs to be routed to both Ethernet PHYs
      4. 6.1.4 AM261_RGMII1_RXLINK and AM261_RGMII2_RXLINK to be connected to GPIO
    2. 6.2 Revision E2 Appendix
      1. 6.2.1 Revision E2 Changes from E1
      2. 6.2.2 Revision E2 Known Limitations
    3. 6.3 Revision A Appendix
      1. 6.3.1 Revision A Changes from E2
      2. 6.3.2 Revision A Errata
    4.     Trademarks
  12. 7References
    1. 7.1 Reference Documents
    2. 7.2 Other TI Components Used in This Design
  13. 8Revision History

Revision A Changes from E2

The following EVM updates were made for LP-AM261 Revision A.

  • Ethernet
    • On-board DP83869 Gigabit PHYs: Revision A of the LP-AM261 removes the Ethernet add-on board ecosystem support and now comes with 2x DP83869 gigabit Ethernet PHYs assembled on-board, each with an RJ-45 connector.
  • PMIC
    • Watchdog Disable: The OTP configuration on the TPS65036601 PMIC enables the watchdog timer by default. This timer triggers a reset signal to the AM261x device if left idle for >12 minutes. On Rev A, the watchdog timer is disabled at power-on by connecting the PMIC's GPIO pin (13) to the internal voltage reference VDD_1P8 pin (3) via jumper SH-J1 on J1 pins 1-2, which comes assembled on the EVM by default. This connection sets an internal bit on the PMIC to disable the watchdog timer before the PMIC ramps. To enable the watchdog at power-on, simply remove the jumper on J1 pins 1-2 before applying 5V/3A to the LP-AM261.
    • nINT and GPIO Pin Assignments: The net assignments for PMIC pins 13 (GPIO) and 21 (nINT) have been corrected in Rev A to their intended use case nets. The GPIO pin (13) is connected to the SAFETY_ERRORn pin on the AM261x MCU when SH-J1 is installed on J1 pins 2-3, and the nINT pin (21) is assigned to PMIC_INTn_GPIO0, which connects to GPIO0 on the AM261x MCU. On previous LP-AM261 revisions, these nets were swapped.
  • BoosterPack Pinout Changes
    • Servo Motor Control BoosterPacks: Revision A now supports a wider array of servo motor control BoosterPacks. These pinout changes are shown in Section 2.11.2.
    • BoosterPack Power Supply Pins: The 3V3 supply on pins J1-1 and J5-41, and the 5V0 supply on pins J3-21 and J7-61 are now enabled by default via jumpers installed at PCB assembly on pins 1-2 of J13, J26, and J27.
    • GPIO124 is routed to J6-52 in order to have the CPTS0_TS_SYNC signal accessible on a header.
  • General
    • The GPIO Interrupt Pushbutton is connected to GPIO5 (changed from GPIO124).
    • The IO Expanders can now be reset using PORz.