SPRUJF1D November 2024 – April 2026
The AM261x LaunchPad is powered through a USB Type-C connection. The USB Type-C source must be capable of providing 3A at 5V and advertises the current sourcing capability through the CC1 and CC2 signals. On the AM261x LaunchPad, the CC1 and CC2 nets from the USB Type-C connector are interfaced to the port controller IC (TUSB320). This device uses the CC pins to determine port attach and detach, cable orientation, role detection, and port control for Type-C current mode. The CC logic detects the Type-C current mode as default, medium, or high.
The Port pin is pulled down to ground with a resistor to configure it as upward facing port (UFP) mode. VBUS detection is implemented to determine a successful attach in UFP mode. The OUT1 and OUT2 pins are connected to a NOR gate. Active low on both the OUT1 and OUT2 pins advertises high current (3A) in the attached state which enables the VUSB_5V0 power switch to provide the VSYS_5V0 supply - which powers the PMIC and LDOs.
In UFP mode, the port controller IC constantly presents pull down resistors on both CC pins. The port controller IC also monitors the CC pins for the voltage level corresponding to the Type-C mode current advertisement by the connected DFP. The port controller IC de-bounces the CC pins and waits for VBUS detection before successfully attaching. As a UFP, the port controller device detects and communicates the advertised current level of the DFP to the system through the OUT1 and OUT2 GPIOs.
The AM261x LaunchPad power requirement is 5V at 3A. If the source is not capable of providing the required power, the output at the NOR gate becomes low and disables the VUSB_5V0 power switch. Therefore, if the power requirement is not met, all power supplies except VCC3V3_TA remain in the off state. The board gets powered on completely only when the source can provide 5V at 3A.
Figure 2-3 Type-C CC Configuration| OUT1 | OUT2 | Advertisement |
|---|---|---|
| H | H | Default current in unattached state |
| H | L | Default current in attached state |
| L | H | Medium current (1.5A) in attached state |
| L | L | High current (3.0A) in attached state |
The AM261x LaunchPad system power solution is PMIC-based. The on-board PMIC supplies the output of its three buck converters and one LDO regulator for each of the power rails. The PMIC generates the supplies required for the AM261x microcontroller and all other EVM peripherals. During the initial stage of the power supply, 5V supplied by the type-C USB connector is used to generate all of the necessary voltages required by the LaunchPad.
| Component | Reference Designator | Function | Voltage In | Voltage Out |
|---|---|---|---|---|
| TPS650360 | U28 |
|
|
|