SPRY356 October 2026 ADS7142 , DRV8426
The liquid-to-liquid architecture, shown in Figure 4, uses direct-to-chip cold plates to absorb heat at the source and coolant distribution units (CDUs) to circulate fluid and transfer heat from one liquid to another and from the white space to the outdoors, where it's released.
Figure 4 Liquid-to-liquid cooling
architectureThe CDU is the most important component in the liquid-to-liquid architecture, keeping fluid flowing so heat is absorbed effectively, and components stay within their intended temperature range. The heat exchanger inside the CDU is equally vital, isolating the low-impurity, high-specific-heat liquid that absorbs heat from the cold plates from the facility water used in the outdoor cooling systems.