SPRZ569F November 2024 – August 2026 F29H850DM , F29H850DU , F29H850TU , F29H859TU-Q1 , F29P329SM-Q1 , F29P580DM , F29P589DM-Q1 , F29P589DU-Q1
MEMSS: Data Line Buffer (DLB) for RAM Causes Data Coherency Issue
0, A, B, C
When the Data Line Buffer (DLB) is enabled (by default) and two CPUs perform simultaneous read/write operations to the same RAM address location, the read operation may receive stale data instead of new data in certain conditions.
The user should disable the DLB using the configuration bit in the MEM_DLB_CONFIG register if the RAM block is shared between multiple CPUs.