SPVA076 October   2026 LP8864-Q1 , LP8866-Q1 , LP8866S-Q1 , LP8872-Q1 , LP8873-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Inductor Acoustic Noise and Designs
  6. 3Capacitor Acoustic Noise and Solutions
  7. 4Summary
  8. 5References

Capacitor Acoustic Noise and Solutions

In LED driver circuits, capacitor acoustic noise is mainly induced by the LED PWM frequency. As listed in Table 3-1, the relationship between LED PWM frequency and dimming resolution for the LP8866-Q1 driver is shown. Theoretically, audible noise can occur when the LED PWM frequency falls within the human-audible range (20Hz to 20kHz). However, in practical implementations, the magnitude of acoustic emissions correlates with multiple factors including output current, dimming mode, PCB layout, and capacitor type. Upon detection of audible capacitor noise, a modest reduction in dimming resolution can be implemented to elevate the LED PWM frequency beyond the audible threshold. Nevertheless, dimming resolution requirements typically impose an upper limit on LED PWM frequency. Subsequent sections addresses mitigation strategies for scenarios where the LED PWM frequency is constrained to a fixed value.

Table 3-1 LED PWM Frequency and Dimming Resolution on LP8866-Q1
R_PWM_FSET (kΩ) LED PWM Frequency (Hz) PWM Dimming Resolution (Bits)
3.92 152 16
4.75 305 16
5.76 610 15
7.87 1221 14
11 2441 13
17.8 4883 12
42.2 9766 11
124 19531 10

LED drivers typically offer multiple dimming modes. For LP8866-Q1, three operational modes are available: PWM dimming, analog dimming, and hybrid dimming. Among these, PWM dimming and hybrid dimming are mainly employed in practical applications. As illustrated in Figure 3-1 and Figure 3-2 (where the upper trace represents the PWM input signal and the lower trace depicts the LED current waveform), distinct operational characteristics are observed.

In PWM dimming mode, the LED current waveform strictly follows the input PWM duty cycle, while the switching frequency is determined by the R_PWM_SET resistor configuration. Notably, in high-current applications, piezoelectric effects become more pronounced, thereby increasing susceptibility to audible noise generation.

Conversely, hybrid dimming operates as follows: When the input PWM duty cycle exceeds 12.5%, the LED current maintains a constant value proportional to the input duty cycle. Only when the input duty cycle falls below 12.5% does the system transition to PWM operation at 12.5% of the maximum current. This methodology confers dual advantages: At high currents, the constant-current operation eliminates both audible noise and visible flicker; at low currents, the controlled PWM operation ensures consistent LED luminance while mitigating severe piezoelectric effects inherent in conventional PWM dimming.

The strategic implementation of hybrid dimming thus resolves the fundamental trade-off between noise suppression and dimming precision in LED driver applications. Therefore, upon detection of acoustic noise emissions during PWM dimming operation, implementation of hybrid dimming mode is recommended as a mitigation strategy. Hybrid dimming is the first choice if there is no other concern.

 LP8866-Q1 PWM Dimming ModeFigure 3-1 LP8866-Q1 PWM Dimming Mode
 LP8866-Q1 Hybrid Dimming ModeFigure 3-2 LP8866-Q1 Hybrid Dimming Mode

The latest LP8872-Q1 LED driver from Texas Instruments incorporates a proprietary enhanced pulse-width modulation (EPWM) algorithm specifically engineered to attenuate audible noise emissions while maintaining fixed dimming resolution. This innovation is activated via configuration of the EPWM_MODE bit within the device register configuration.

Besides the reason related to the dimming frequency, another possible cause of capacitor audible noise is an excessively high input voltage.

BOOST devices all have a minimum on-time. As the voltage differential between the input and output decreases, the on-time per switching cycle becomes shorter. Once this minimum on-time is triggered, the device maintains output voltage regulation by reducing the switching frequency. This is how PFM works, as shown in Figure 3-3. When the reduced switching frequency falls within the audible range of the human ear, it results in audible noise.

 Switching Frequency in LP8866-Q1 PFMFigure 3-3 Switching Frequency in LP8866-Q1 PFM

In some applications, the input voltage test range is 9–22V. According to the datasheet, the minimum switching time of LP8866-Q1 is 150ns. At a switching frequency of 400kHz and an output voltage of 24V, the maximum input voltage is approximately 21V, which cannot meet the requirement. In this case, LP8872-Q1 can be considered, since its minimum switching time is 60ns, corresponding to a maximum input voltage of approximately 22.5V.

Besides switching to a device with a smaller minimum switching time, the issue can also be addressed by increasing the output voltage. Taking an output voltage of 24V as an example, if the output voltage needs to be increased by 1V, since the LED driver's output is a current source, the resistor can be selected by determining the maximum output current. Assuming each LED channel has a maximum of 90mA, the maximum VLED current for six channels is 540mA, which requires a resistor of approximately two ohms. Considering high-temperature testing and heat dissipation concerns, three 6.8ohm resistors in 1206 package connected in parallel are selected here, as shown in Figure 3-4. If you plan to use this approach, please contact TI technical support and carefully consider the resistor value and package size.

 External Resistor on
                              VLED Figure 3-4 External Resistor on VLED

From the layout and capacitor selection side, there are several PCB layout techniques that can effectively mitigate audible noise emissions in LED driver circuits. As illustrated in Figure 3-5, where multiple ceramic capacitors are typically deployed at the driver output stage, an orthogonal placement configuration of adjacent MLCCs is recommended. Specifically, arranging two capacitors at 90° relative orientation attenuates the cumulative piezoelectric effect through counteracting mechanical displacements. This geometric countermeasure reduces the net vibrational amplitude by inducing opposing strain vectors in the ceramic dielectric layers, thereby suppressing acoustic emissions within the human-audible frequency range.

 Ceramic Capacitors LayoutFigure 3-5 Ceramic Capacitors Layout

In PCB layout design, the implementation of symmetric capacitor placement across opposing substrate surfaces constitutes an effective noise suppression strategy. Furthermore, augmentation of the PCB substrate thickness (for example, ≥1.6mm) is empirically validated to mitigate audible emissions through mass-stiffness modification of the structural resonance profile.

 Capacitors on Both Sides of PCBFigure 3-6 Capacitors on Both Sides of PCB

In capacitor selection methodology, audible noise suppression can be achieved through two primary approaches: substitution of ceramic capacitors with electrolytic alternatives, or implementation of specialized ceramic capacitor designs. As depicted in Figure 3-7, engineered multi-layer ceramic capacitors (MLCCs) featuring mechanically isolated mounting configurations exhibit substantially attenuated piezoelectric effects. This attenuation occurs through decoupling of mechanical vibrations from the printed circuit board (PCB) substrate, as the capacitor terminals do not establish direct physical contact with the PCB surface. Consequently, the transmission path for strain-induced acoustic emissions is disrupted, resulting in significantly reduced audible noise generation.

 Specialized Ceramic CapacitorsFigure 3-7 Specialized Ceramic Capacitors

Alternatively, strategic replacement of ceramic capacitors with electrolytic counterparts in non-critical decoupling positions can eliminate piezoelectric noise sources entirely, though this approach necessitates careful consideration of equivalent series resistance (ESR) characteristics and lifetime implications. The selection between these methodologies must be informed by rigorous analysis of circuit requirements, thermal constraints, and acoustic performance specifications.