SSZTAT1 october 2016
I started working at Texas Instruments in the late-1980s, a time after Dr. Larry Hornbeck invented the digital micromirror device (DMD) in 1987. The overall development of microelectromechanical systems (MEMS) upon which DLP® chips are based was still in its infancy.
With MEMS as a framework, the broad array of DLP technology applications that we see today – everything from advanced light control, to portable projection displays and automotive solutions – had not yet even been considered.
The micromirror design we worked on at that time was very simple. It consisted of 840 micromirrors and two hinges that connected to the micromirror itself. The micromirror had 4 access holes to allow for sacrificial layer removal. To say the least, this micromirror was not as optically efficient as the DMDs we use today.
Early DMD micromirror design
That was when we realized the DMD – a layered MEMS chip gleaming with thousands of light-bending microscopic mirrors – could change how the world interacts with video projection and displays. Thus, if we could productize a device with 840 micromirrors, we could certainly productize a device with millions of micromirrors.
Consider this: While solid-state solutions struggle to detect environmental inputs like motion, pressure, sound and chemical sensing, MEMS solutions, like a DMD, really shines. That’s because MEMS combine the best of macromechanical solutions and solid-state technology in a smaller, lower cost and high performance form factor. A non-DMD example would be the integration of a MEMS device, such as a Silicon MEMS microphone and its associated electronics, which provide a robust and reliable solution for consumer electronics compared to its macro-counterpart.
We’re now focused on delivering DLP chips with a variety of performance characteristics, such as faster switching speeds, to enable diverse end equipment.
The co-location of our design, product and process teams allows for fast development cycles as we continue to improve our products.
MEMS technology, like our DLP technology, is poised to find more uses than ever before. From intelligent smart home displays to next-generation augmented reality, the work from TI, our partners and customers are already a shining example of innovation.