SWRA475A January 2015 – October 2016 CC2540 , CC2540T , CC2541 , CC2541-Q1
The TI Packet Sniffer was used to test the device. Figure 11 shows an advertising packet as it was discovered by the sniffer. It can be seen that the advertising data reflects the requirements of the iBeacon specifications, as does the advertising PDU type.
Figure 11. Sniffer Packet Showing the Advertising Data of the Beacon Device