SWRA657 June 2020 CC3100 , CC3200
Before diving into the file system structure, it is highly important for designers to understand how content is created on the serial flash.
There are several ways for files to be created on the serial flash. Table 1 describes the various options.
| Application/Tool | Device State | Content Delivery Channel | Content Type | Package/Example |
|---|---|---|---|---|
| Uniflash | Bootloader | UART | User, system and configuration files | SimpleLink Wi-Fi CC3100, CC3200 UniFlash User's Guide (SWRU558) |
| SimpleLinkTM file system API | Operational | UART/SPI | User files |
|
| SimpleLink non file system API | Operational | UART/SPI | System and configuration files | Any SDK example using the SimpleLink host driver |
| SimpleLink Device internals | Operational | Device internals | N/A |