SWRA657 June 2020 CC3100 , CC3200
In an AC line powered system, the failure of the grid can cause the supply of the Wi-Fi subsystem to drop suddenly. In the unlikely event this coincides with the erase operation of the serial flash, there is a chance of data corruption. One of the ways to minimize the chance of a flash corruption would be to ensure that the DC voltage ramps down slowly after the input power is removed. This can be achieved with the help of bulk capacitors which hold the charge while input supply is removed. The embedded system would sense the sudden fall in the input voltage and then initiate a soft shutdown of the Wi-Fi sub-system thereby safely completing all serial flash operations before Vflash-min is reached. The charge stored on the capacitor would be used during this brief interval. Such a sequence is illustrated in Figure 6.
Figure 6. Serial Flash Corruption Avoided Through Use of a Bulk Capacitor