SWRA715 December 2021 CC2642R , CC2652R
The HOGP specification states that the connection interval for device that implements the HOGP must be in the range of 7.5 ms to 50 ms. This project implements a 7.5 ms connection interval by default, but this can be changed to another value if desired. For more information on how to change the connection interval, please refer to the SDK User’s Guide. A connection interval of 7.5 ms provides the fastest response time and lowest latency for the hid_emu_kbd. Figure 4-5
Figure 4-5 Bluetooth Traffic Log Snippet
Showing 7.5 ms Connection IntervalThe connection interval is very important to performance because the HID input data is sent to the HID Host via notifications that can only occur during a connection event.