SWRU498B February   2017  – December 2021 CC2564C

 

  1.   Trademarks
  2. Features
  3. Bluetooth Profiles
  4. Sample Application Overview
  5. CC2564CSTBTBLESW Hardware and Software Requirements
  6. Setting Up the Hardware
  7. Setting Up the Software
  8. Building and Flashing the Bluetooth Code (STM3240G-EVAL)
    1. 7.1 Flashing the Bluetooth Code
  9. Applications
  10. Classic Bluetooth Sample Applications
  11. 10Classic Bluetooth + Bluetooth Low Energy Applications
  12. 11Bluetooth Low Energy Applications
  13. 12Revision History

Flashing the Bluetooth Code

STSW-LINK004

You can use the STSW-LINK004 utility to flash the software when you have created the binary file through IAR or Keil.

To flash the software, do the following:

  1. Open the file from the File drop-down menu.
  2. Select the demonstration to load on the device. (This example uses SPPDemo.)
    • For NoOS, navigate to C:\TI\Connectivity\CC256XBT\CC256xSTM32BluetopiaSDK\v4.2.x.x\NoOS\STM3240G-EVAL\Samples\SPPDemo\NoOS\EWARM\Debug\Exe.
    • For FreeRTOS, navigate to C:\TI\Connectivity\CC256XBT\CC256xSTM32BluetopiaSDK\v4.2.x.x\FreeRTOS\STM3240G-EVAL\Samples\SPPDemo\FreeRTOS\EWARM\Debug\Exe.
  3. Select a bin file. (This example uses SPPDemo.bin.)
  4. Click Program & Verify... from the Target drop-down menu. (See Figure 7-10.)
    GUID-EDD15013-8BDA-4076-A22D-3BA089BDD730-low.gif Figure 7-10 Program and Verify
    Note: The information for your device shows.
  5. Ensure the values in Device Information changed to your device information.
  6. Press Start. (See Figure 7-11.)
    GUID-D931970C-9629-40D6-87CE-815B25B935EA-low.gif Figure 7-11 Start Download
    Note: The command window displays Verification...OK. (See Figure 7-12.)
    GUID-0D680501-DEA2-4C92-A427-EA37E09ED1A4-low.gif Figure 7-12 Verification...OK