SWRU529C May 2017 – April 2020
One of the commands sent caused the software running on the device to crash and an assert or exception message is displayed in the console messages. Users can connect the CCS debugger to the target device to debug this situation further. In the absence of CCS, reboot the device and start again. If the device still does not work for a given config, check the config against the mmWave SDK user's guide. One reason could be that the number of plots selected caused the shipment of the output data to exceed one frame duration.
Another reason could be the mismatch between the baud rate selected for DATA_port in the Visualizer versus the rate at which device is transmitting (mmWave SDK 3.4 and later). To address this, reboot the sensor or stop the sensor, re-connect the serial ports from Visualizer GUI with desired baud rate and reconfig the sensor.