SWRU529C May 2017 – April 2020
This plot shows the detected objects using the range and Doppler coordinates (see Figure 8). For the advanced frame, this plot shows the union of points detected in all subframes of a given frame.
NOTE
Select Scatter Plot in the Configure tab and configure the device accordingly to view this plot.
The X-axis can be controlled using the Range Width and Range Depth text boxes. Use the stop button to stop plotting and then you can change these settings. When changed, resume the plotting using the start button. The maximum value users can select is limited by the Maximum Unambiguous Range achievable by the current configuration.
Figure 8. Doppler Range Plot for Detected Objects