SWRU613A July   2023  – August 2024

 

  1.   1
  2.   Description
  3.   Get Started
  4.   Features
  5.   5
  6. 1Evaluation Module Overview
    1. 1.1 Introduction
    2. 1.2 Kit Contents
    3. 1.3 Specification
    4. 1.4 Device Information
  7. 2Hardware
    1. 2.1  XWRL1432BOOST Antenna
      1. 2.1.1 PCB Material
        1. 2.1.1.1 Transmitter and Receiver Virtual Array
    2. 2.2  EVM Mux Block Diagram
    3. 2.3  Switch Settings
    4. 2.4  LEDs
    5. 2.5  Connectors
    6. 2.6  USB Connector
    7. 2.7  DCA1000 HD Connector
    8. 2.8  Booster Pack Connector for the LaunchPad Connectivity
    9. 2.9  CANFD Connector
    10. 2.10 LIN PHY Connection
    11. 2.11 I2C Connections
      1. 2.11.1 EEPROM
    12. 2.12 XDS110 Interface
    13. 2.13 Flashing the Board
    14. 2.14 DCA1000EVM Mode
      1. 2.14.1 RDIF Interface for Raw ADC Capture
    15. 2.15 PCB Storage and Handling Recommendations:
      1. 2.15.1 PCB Storage and Handling Recommendations
      2. 2.15.2 Higher Power Demanding Applications
  8. 3Software
    1. 3.1 Software, Development Tools, and Example Code
      1. 3.1.1 XWRL1432 Demo Visualization Getting Started
  9. 4Hardware Design Files
    1. 4.1 Schematics, PCB Layout and Bill of Materials (BOM)
    2. 4.2 EVM Design Database
  10. 5Additional Information
    1. 5.1 Trademarks
  11. 6References
    1. 6.1 TI E2E Community
  12. 7Revision History

XWRL1432 Demo Visualization Getting Started

xWRL1432BOOST Demo Visualization Getting
          Started Figure 3-1 Demo Visualization Getting Started

Prerequisites:

  1. Download latest SDK package of MMWAVE-L-SDK.
  2. Download latest XDS110 drivers. This is bundled with Code Composer Studio (CCS).

Steps for getting started:

  • Step 1: Connect the EVM to the micro USB port. Users do not need to connect to the barrel jack.
  • Step 2: Navigate to the MMWAVE-L-SDK download location and run the Low Power Radar Visualizer. The visualizer is located in <MMWAVE_L_SDK_5_INSTALL_DIR>\tools\visualizer\Low_power_visualizer_5.x.x.x\visualizer.exe
  • Step 3: Connect the EVM to the PC via USB. Users do not need to connect to the barrel jack.
  • Step 4 (Optional): Program a non-default firmware / app-image.
    1. Navigate to the Flash tab.
    2. AUTO detect COM ports (press refresh icon) and select device COM port (if not already selected).
    3. Follow the subsequent steps shown in the Visualizer.
  • Step 5: Configure Device
    1. Navigate to the Configuration Dashboard tab.
    2. AUTO detect COM ports (press refresh icon) and select device COM port (if not already selected).
    3. Select preset configuration under Configuration Selection.
    4. Click on Send Selected Config.
  • Step 5: Plots tab displays point cloud information.