TIDUE18 November 2022 TPS51215A
IMON output is needed by IMVP multiphase VR controller. IMVP controller has related pins for the input and they should be connected with the IMON output from VCCIN_AUX solution.
Currently, there are two major types of IMON output signal, which is determined by the used IMVP VR controller:
The schematic design is shown as Figure 2-2.
Figure 2-2 TPS51215A Power Solution with
Load Line Feature SchematicFigure 2-2 is the major page of schematic in this reference design, which only includes the circuits around voltage regulator. The symbol for test tool interposer and the output capacitors placed at loading side (interposer side) are not shown here.
The complete schematics of the reference design are at TIDA-050057.
The principle for implementation will be introduced in Section 2.4.