TIDUE59A May 2018 – September 2020
The experimental results from Section 3.2.4 can be used to estimate the battery life of a system that is based on this design. Based on the results in Section 3.2.4 and using the assumption that the electronic smart lock is locked or unlocked 24 times per day, users can estimate the power consumed by each subsystem.
The main parameters of the Wi-Fi subsystem that affect the estimated battery life are as follows:
Equation 1 gives the average Wi-Fi idle power.

Equation 2 gives the average Wi-Fi power per day, due to locking and unlocking.

Equation 3 gives the average Wi-Fi power per day, due to the checking lock status.

Equation 4 gives the approximate average Wi-Fi power.

The main parameters of the BLE subsystem that affect the estimated battery life are as follows:
Equation 5 gives the approximate average BLE power.

The main parameters of the motor driver subsystem that affect the estimated battery life are as follows:
Equation 6 gives the average motor driver idle power.

Equation 7 gives the average motor driver power during a lock event.

Equation 8 gives the average motor driver power during an unlock event.

Equation 9 gives the approximate average motor driver power.

Using the calculations for the power consumed by the Wi-Fi, BLE, and motor subsystems, users can estimate the total average system power (see Equation 10).

The estimated total system power can be used to estimate the battery life of the system, using the theoretical energy capacity of the power source. For this estimate, assume an energy capacity of 18,000 mWh and calculate the months of battery life using Equation 11.