TIDUE59A May 2018 – September 2020
When assembling the TIDC-01005 demo, CC3220S-LAUNCHXL, LAUNCHXL-CC2640R2, and BOOSTXL-SENSORS must all be connected by stacking the 20-pin headers on the EVMs in the following order (with 1 being the top of the stack and 3 being the bottom).
When the LaunchPads and BoosterPack are stacked, ensure the 2-pin jumper is placed horizontally across J4-J6 and J2-J6 on the sensor BoosterPack, to connect pin 7 of the CC3220S and BPRST of the CC2640R2F. Figure 3-5 shows how the assembly appears.
Figure 3-5 LaunchPad™ and BoosterPack™ StackupLast, connect the stackup to the DRV8837EVM according to Table 3-3 using the jumper wires (connections shown in Figure 3-6). The entire system can be powered by connecting the USB cable to the USB connector on the CC3220S LaunchPad.
Figure 3-6 Jumper Wire Placement to Connect DRV8837EVM to System