TIDUED6B august 2018 – april 2023
The CC1352 device configures the IWR6843 device via a command line interface (CLI) UART port. After the configuration is completed, the IWR6843 starts sending out radar data continuously back to CC1352 through a separate data UART port. Then, the CC1352 parses the data from the IWR6843 and packetizes and sends the data package over the air to the collector node constantly. Figure 2-3 is a block diagram of the IWR6843 UART communication.
Figure 2-3 IWR6843 UART Communication