TIDUEU6B September 2020 – December 2021 OPA810
When the unknown impedance to be measured is capacitive i.e. CX, it forms the circuit shown in Figure 2-3. The transfer function of VF is given in Equation 4.
Figure 2-7 Capacitive Measurement with Series ResistanceIn comparison with Equation 2, Equation 4 shows that due to presence of RG, there is a pole-zero combination in the feedback path. The zero and pole frequencies in 1/β are given by,
The pole and zero frequencies hold the relation ωP = 2*ωZ because RG is equal to RF in every RG - RF setting.
Figure 2-8 Bode Plot of Capacitive
Measurement with Series ResistanceThis provides the advantage of an inherent pole to cancel the zero. Figure 2-8 shows that the rate of closure of Aolβ is 20 dB/dec for almost all the CX. The exception for this fact is when fCL lies between fZ and fP. The RG - RF settings are selected such that this situation is avoided. This allows for a key factor of this design where ωP = 2*ωZ is independent of the value of CX. The measurement can be done in two ways as explained below,