TIDUEX2 July 2020
Figure 2-4 Designing Buck Converter Circuit TPS62864To support a simple evaluation, a tantalum input capacitor C3 is used to ensure a steady, low-impedance supply voltage for the ICs.
Also, to achieve a smaller package size, the GRM155R60J226ME11 22uF 0402 capacitors were used in C2, C4, and C5. The recommended minimum input capacitance for this device is 8uF. According to the characteristics of this capacitor, this would mean that the maximum input voltage should be 3.3 V to ensure that C2 effective capacitance is 8uF. Similar considerations were applied for the TPS62088 designs.