TIDUEY3 November 2020
The Occupancy Detection State Machine is the processing that examines the detections within each zone and makes yes or no occupancy decisions each frame. Figure 2-9 shows the steps algorithm goes during each frame call.
All condition parameters and thresholds are configurable via CLI interface. The values used in the application demo and the state machine are not definitive. Continued improvements and customization of the state machine is recommended to fine-tune the processing to fit application needs.
Figure 2-9 Zone State Machine