TIDUF64C December 2023 – July 2026
Figure 4-3 shows the voltage of the switching node of the H-Bridge with unipolar modulation scheme. The image shows that no important overvoltage is detected even when the switching is at 60kV/μs, with a rise time of around 25ns.
The voltage of the switching node of the H-bridge with bipolar modulation scheme is measured as shown in Figure 4-18. The image shows that no important overvoltage is detected even when the switching is at 60kV/μs, with a rise time of around 25ns.
Figure 4-19 shows the voltage of the switching node of the HERIC modulation scheme. From a topology point of view, in HERIC mode, due to additional zero-voltage states in positive and negative half-cycles, the voltage across the FETs is also halved. The switching node voltage rises from 200V to 400V. The other switching node in this scenario ranges from 0V to 200V.