TIDUF78 May 2024
The serial-data-in (SDI) line is used by the host controller to configure the TMAG5170 registers, start a new conversion, or send a read command. The SDI bits are latched with each SCLK rising edge when the nCS pin is low. Figure 3-2 explain the SDI frame. There are 4 command bits in the SDI line to select the status bit for the next frame or start a new conversion.