TIDUFH5 March 2026 TPSI31P1-Q1
Optimize the high di/dt loop by placing the input capacitance close to the switching circuit. Figure 4-2 illustrates the main reference design current loops using a simplified schematic and the reference design layout.
|
Figure 4-2 High di/dt Loop Schematic and
Layout
|
|
In this circuit, S1 represents the MOSFET and S2 represents the flyback diode. Current alternates between the S1 and S2 paths; the current remains continuous where these loops overlap but is discontinuous in the non-overlapping section. This results in a high di/dt loop as the current suddenly transitions from zero to the full load current. Parasitic inductances and capacitances within this loop form resonant circuits that generate voltage oscillations during transitions, as shown in Figure 4-3. Excessive oscillations can exceed absolute maximum specifications, potentially damaging the MOSFET or flyback diode.
Reducing the high di/dt loop length minimizes the energy stored and released by parasitic elements (WL = 0.5 × LI2) and reduces voltage overshoot (VL = L × diL/dt). Additionally, current in this loop forms a time-varying H-field which can inject current into nearby circuits through mutual inductance, causing more EMI. Minimize the high di/dt loop length and place the input capacitance as close as possible to the MOSFET drain and flyback diode anode for best performance.
If excessive VSW oscillations persist, consider increasing damping by implementing: