TIDUFJ8 July   2026

 

  1.   1
  2.   Description
  3.   Resources
  4.   Features
  5.   Applications
  6.   6
  7. 1System Description
  8. 2System Overview
    1. 2.1 Block Diagram
    2. 2.2 Design Considerations
      1. 2.2.1 Design Considerations Introduction
      2. 2.2.2 Basic Operation Principles for DAB
    3. 2.3 Highlighted Products
      1. 2.3.1 TMS320F28P550SG
      2. 2.3.2 TMCS1126
      3. 2.3.3 UCC23525
      4. 2.3.4 UCC27834
      5. 2.3.5 AMC03111R
    4. 2.4 System Design Theory
      1. 2.4.1 Switching Frequency and Transformer Ratio Design
      2. 2.4.2 Resonant Inductance Design
      3. 2.4.3 DC-Blocking Capacitor Design
      4. 2.4.4 Hardware Design Theory
        1. 2.4.4.1 Power Stage
        2. 2.4.4.2 Sensing
  9. 3Hardware, Software, Testing Requirements, and Test Results
    1. 3.1 Hardware Requirements
    2. 3.2 Test Setup
    3. 3.3 Test Results
  10. 4Design and Documentation Support
    1. 4.1 Design Files
      1. 4.1.1 Schematics
      2. 4.1.2 BOM
    2. 4.2 Tools and Software
    3. 4.3 Documentation Support
    4. 4.4 Support Resources
    5. 4.5 Trademarks
  11. 5About the Author

Basic Operation Principles for DAB

The Single-Phase-Shift (SPS) modulation is the most fundamental and widely adopted control method for the Dual Active Bridge (DAB) converter. Under SPS control, both the primary-side full bridge (Bridge 1) and the secondary-side full bridge (Bridge 2) operate at a fixed 50% duty cycle. The diagonal switch pairs of each bridge (such as Q1/Q4 and Q5/Q8) are turned on and off synchronously .

The core control variable in this scheme is the external phase-shift angle ϕ introduced between the primary-side square-wave voltage (Vp) and the secondary-side square-wave voltage (Vs). This phase shift angle directly regulates the direction and magnitude of the power flow across the high-frequency isolation transformer T1, as shown in Figure 2-4.

TIDA-010990 Waveforms under SPS
                    control Figure 2-4 Waveforms under SPS control

The average power P12 transferred between the two bridges is governed by the energy stored and released in the series leakage inductor Ls, which can be mathematically expressed as :

Equation 1. P 12 = N · V 1 · V 2 · ϕ · ( π - | ϕ | ) 2 · π 2 · L s · f s    ( - π ≤ ϕ ≤ π )

Where V1 is the input DC voltage, V2 is the output DC voltage, fs is the switching frequency, and N is the transformer turns ratio (N = N1/N2) .

  • Forward Power Mode ( 0 ≤ ϕ ≤ π ): Vp leads Vs, causing energy to flow from the primary side to the secondary side .
  • Reverse Power Mode ( - π ≤ ϕ ≤ 0 ): Vp lags Vs, causing energy to seamlessly flow back from the secondary side to the primary side.
The maximum power capability (Pmax) is strictly limited by the hardware parameters Ls and fs, and is achieved when the phase-shift angle ϕ equals π / 2 :
Equation 2. P m a x = N · V 1 · V 2 8 · L s · f s
TIDA-010990 Complete Waveforms of PWM and Current Under SPS Control Figure 2-5 Complete Waveforms of PWM and Current Under SPS Control

To minimize switching losses and achieve high total system efficiency, the SPS-DAB relies entirely on the reactive energy stored in the leakage inductor Ls to discharge and charge the MOSFET parasitic output capacitances Coss, thereby facilitating Zero Voltage Switching (ZVS). Figure 2-5 shows complete waveforms of PWM and current . Taking the forward operation mode as a reference, a typical switching cycle progresses through the following key intervals:

  • Interval 1 ( t 0 to t 0 ' - Dead Time Realization, as shown in Figure 2-6): Prior to t 0 , the switches Q1 and Q4 are turned off . During this dead-time interval, the inductor current IL must remain negative ( I L ( t 0 ) < 0 ). This negative current forces the energy stored in Ls to discharge the output capacitances of Q1 and Q4 while charging those of Q2 and Q3, creating the necessary zero-voltage condition across Q1 and Q4 prior to their turn-on .
    TIDA-010990 DAB converter operating stage during Interval 1 Figure 2-6 DAB converter operating stage during Interval 1
  • Interval 2 ( t 0 ' to t 1 - Primary Channel Conduction, as shown in Figure 2-7): At t 0 ' , switches Q1 and Q4 are turned on under a strict zero-voltage condition(Ideal situation). The inductor current passes through the channels of Q1 and Q4, and begins to rise linearly .
    TIDA-010990 DAB converter operating stage during Interval 2 Figure 2-7 DAB converter operating stage during Interval 2
  • Interval 3 ( t 1 to t 2 - Current Reversal, as shown in Figure 2-8): At t 1 , the inductor current crosses zero and switches its direction to positive, continuing its linear progression driven by the voltage difference across the transformer.
    TIDA-010990 DAB Converter Operating Stage During Interval 3 Figure 2-8 DAB Converter Operating Stage During Interval 3
  • Interval 4 ( t 2 to t 2 ' - Secondary Side ZVS Realization, as shown in Figure 2-9): At t 2 , the secondary side switches Q5 and Q8 are turned off . To enable ZVS for the secondary bridge, the inductor current at this moment must be positive ( I L ( t 2 ) > 0 ). This positive transformer current successfully discharges the output capacitances of Q5 and Q8 while charging Q6 and Q7 during the secondary side dead time.
    TIDA-010990 DAB Converter Operating Stage During Interval 4 Figure 2-9 DAB Converter Operating Stage During Interval 4
  • Interval 5 ( t 2 ' to t 3 ) - Full Commutation, as shown in Figure 2-9): At t 2 ' , Q5 and Q8 achieve soft turn-on. The current flows naturally through the secondary bridge channels, completing the primary-to-secondary power commutation phase until the next half-cycle repeats the identical process for the remaining FETs from t 3 to t 6 .
    TIDA-010990 DAB Converter Operating Stage During Interval 5 Figure 2-10 DAB Converter Operating Stage During Interval 5