>> Semiconductor Home > News and Publications >

news releases

   Semiconductor News and PublicationsGray Rule

   Related Documentation:
> DSP Products

> TI Delivers 600 MHz DSPs
   Giving Wireless, Broadband
   and Imaging Designers Up
   To 15X the Performance with
   1/3 Power Dissipation

> TMS320C64x™ Customer
   Quote Sheet

> Texas Instruments
   TMS320C64x™ Digital
   Signal Processors

> TMS320C64x™ Sampling
   Announcement

> News Releases

publications
> Technology Innovations
> Sine On Analog and Mixed-
   Signal Catalog

trade shows
> Current Trade Shows

search news archives
> Search the News Archives

 

TI Delivers 600 MHz DSPs Giving Wireless, Broadband and Imaging Designers Up To 15X the Performance with 1/3 Power Dissipation

Three new programmable DSPs are among the first TI products developed in 0.13 micron copper process technology

TMS320C6416; TMS320C6415; and TMS320C6414 DSP chipsets HOUSTON (September 10, 2001) -- Delivering the highest-performing DSPs to date, Texas Instruments Incorporated (TI) (NYSE: TXN) announced that customers have begun designing products with the first devices based on its TMS320C64x(tm) DSP core, which combines the highest performance and lowest power consumption of any available digital signal processor (DSP). Operating at up to 600 MHz and consuming less than one watt (W) of power, the new devices deliver up to ten times the performance in wireless and broadband applications and up to 15 times the performance in advanced imaging applications, with one third the power dissipation of other single core DSPs. http://www.dspvillage.ti.com/c64xpromo1

"TI continues to accelerate the pace of technological development," said Tom Engibous, TI chairman, president and chief executive officer. "These three new programmable DSPs set the industry benchmark at 600 MHz and are among TI's first products developed in 0.13 micron copper process technology. The C64x™ DSPs have broad capabilities and especially will enable wireless multimedia communications and the full convergence of video, voice and data on all types of broadband networks. Plus, they use just a fraction of the power of today's most advanced DSPs, and our development tools enable the creation of new applications at unprecedented speed. The technology mantra is still 'more, better, faster, cheaper, with less power consumption.' The new C64x DSPs deliver on those demands."

Since the introduction of the TMS320C6414, TMS320C6415 and TMS320C6416 DSPs in February of this year, the new C64x devices have gained broad-based industry acceptance. Dozens of customers and more than 20 third-party developers are designing these devices into advanced imaging, wireless and broadband systems. Customers adopting the new C64x DSPs include: AltiGen Communications, Artel Video Systems, Ericsson, Hewlett Packard, Lucent Technologies, Nortel Networks, Scopus Network Technologies, and Spectel. Third parties developing with C64x include: A.T.E.M.E., Commetrex, Imagine Technology LLC, Motorola, Pentek, Spectrum Signal Processing and Wintegra.

"It is refreshing to see a company deliver the performance they promised at the time of their new product announcement. TI announced their C64x DSPs at 600 MHz and they are actually shipping parts at that speed, making the family the highest-performing, single-core programmable DSPs available today," said Will Strauss, president of DSP market watcher Forward Concepts. "OEMs will be encouraged that TI does not take a 'one size fits all' approach with its products, since they are offering three versions of the new DSP, each tailored for a specific class of applications."

TMS320C6416 DSPs Deliver 10X More Performance for Wireless Infrastructure

The three devices are targeted for specific applications. The C6416 DSP, the most highly integrated of the three, features the on-board coprocessors needed to handle the dense channel capacity of third-generation (3G) wireless base stations. The low power dissipation and exceptional channel density of the C6416 DSP enable wireless infrastructure developers to meet the demanding challenges of third-generation services with the lowest possible cooling requirements.

The C6416 DSP builds on the performance of TI's TMS320C6203 DSP, the industry's previous performance leader which is already being used for base station designs by 80 percent of the top 3G wireless OEMs worldwide. A single 600-MHz C6416 DSP can process up to 350 voice channels at 12.2 kb/s, compared to 74 with the 300-MHz C6203 DSP, and 35 data channels at data rates up to 384 kb/s, compared to a single channel with the C6203 DSP. The DSP accomplishes this task through its inherent processing power and through a Viterbi coprocessor (VCP) dedicated to voice processing, and turbo coprocessor (TCP) for data processing. The C6416 DSP is the only device available today that integrates these essential coprocessors on the chip.

TMS320C6415 DSPs Deliver More Channel Density for Broadband and Imaging

Customers designing advanced broadband communications infrastructure and imaging systems are using the C6415 DSP, which incorporates the same on-chip peripherals as the C6416 DSP but not the wireless-specific coprocessors. "With the 600Mhz processing power of TI's C6415 DSP, and peripherals such as a PCI interface, we are able to quadruple our port density per chip on our VoIP boards as well as accomplish up to 64 channels of voice," said Richard DeSoto, sales and marketing senior vice president, AltiGen. "TI has shown its leadership in the DSP field by continuing to deliver breakthrough products in a timely manner. TI perfectly meets our demands and allows us to stay one step ahead of our competitors in the VoIP market."

The C6415 DSP also provides developers of media gateways and advanced imaging applications the performance and interfaces required to handle multi-channel MPEG-4 video. The DSP can perform one channel of MPEG-4 video encoding, one channel of MPEG-4 video decoding, and one channel of MPEG-2 video decoding, and still have 50 percent headroom remaining for multi-channel voice and data coding. The DSP also features 33-MHz, 32-bit PCI and HPI32 host connectivity for control of interprocessor communications. In addition, the processor supports 50-MHz Utopia Level II ATM connectivity.

"With the delivery of the TMS320C6415, we are able to increase DSP performance by 4x for our MPEG2 decoder and rate reducer applications and still have 50% headroom left over for other tasks such as performance monitoring and communication," said Israel Goldshide, R&D project manager at Scopus Network Technologies. "By delivering the highest performing DSPs and connecting us with TI's third party network, we can continue developing leading edge video products and push them to market quicker than ever."

For developers of systems that do not require dedicated DSP network connectivity, the C6414 DSP provides all of the performance of the 600-MHz C64x core, as well as a host of industry-standard interfaces. Its 64-channel enhanced direct memory access (EDMA) controller delivers unmatched I/O efficiency that manages data transfer from system memory at gigabytes per second. In addition, three multi-channel buffered serial ports (McBSPs) each support 128 time-division multiplex (TDM) channels as well as AC97 and IIS audio interfaces.

High-Performance DSP - Just One Part of an Optimized System

TI provides optimized system solutions along with industry leading DSP and analog parts, software, support, tools, development boards and market knowledge, allowing OEMs to increase revenue by simplifying development and speeding time to market. In addition, TI customers who are designing applications with C64x DSPs can leverage TI digital signal processing support to decrease product development time.

The C64x DSPs are supported by TI's eXpressDSP™ Real-Time Software Technology, including the Code Composer Studio™ v2 Integrated Development Environment (IDE), the industry's most sophisticated DSP IDE and the DSP/BIOS™ real-time kernel. TI's library of DSP and imaging software modules, best-in-class software development tools and eXpressDSP-compliant products from the DSP industry's largest third party network all add up to faster time to market for the designers of broadband and imaging applications. OEMs have begun designs with these three new programmable DSPs, which are software compatible with other members of the TMS320C62x™ DSP platform, allowing developers to port the object code they have developed for earlier designs to the new devices saving valuable design time. The new DSPs are easy to program, and use the C64x DSP compiler that optimizes more than 80 percent of hand-coded assembly.

Availability

TI is scheduled to offer 400, 500, and 600 MHz versions of all three C64x devices. The C6414 DSP pricing begins at $95, C6415 DSP pricing begins at $105, and C6416 pricing begins at $115 in 10,000 unit quantities, all are packaged in 532-lead BGA packages, and are available today. The C64x development boards and complete suite of eXpressDSP development tools are also available today. Technical documentation is available on the Internet at http://www.dspvillage.ti.com/c64xpromo1

# # #

TRADEMARKS
All trademarks and registered trademarks are the property of their respective owners.