Seleccione una versión
DDR-CONFIG-AM62P
DDR Configuration Tool
Productos
SoC de redes industriales y multimedia
Desarrollo de hardware
Placa de evaluación
Documentación
Link to DDR Register Configuration Tool
Información de la versión
This tool is intended to simplify the process of configuring the DDR Subsystem Controller and PHY to interface with DRAM memory devices.
The DDR Register Configuration tool can be downloaded and installed on your local workstation by following these instructions:
- Install SysConfig
- Download the latest Sysconfig from https://www.ti.com/tool/SYSCONFIG
- Run the installer and install to `c:\ti` for windows or `~/ti` for linux
- Install the DDR RegConfig Tool:
- Open Resource Explorer at https://dev.ti.com/tirex/explore
- Select the menu (icon with 3 horizontal lines) in the upper right and choose Package Manager
- Scroll until you see DDR Configuration for AM64x, AM625, AM623, AM62Ax, AM62Px, AM62Dx
- Select More and choose the latest version to download
- You should now have a zip file `Processor_DDR_Config_\<version\>_all.zip` Extract the zip to `c:\ti` for windows or `~/ti` for linux.
- Run the tool with the following command after substituting for:
- The SysConfig version,
- The Processor\_DDR\_Config version, and
- The device name if needed (either AM64x, AM62x, AM62Ax, AM62Px, AM62Dx)
Windows command example:
c:\ti\sysconfig_<version>\sysconfig_gui.bat --product c:\ti\Processor_DDR_Config_<version>\.metadata\product.json --device <device name>
Linux command example:
~/ti/sysconfig_<version>/sysconfig_gui.sh --product ~/ti/Processor_DDR_Config_<version>/.metadata/product.json --device <device name>
Novedades
- fixed PI byte swap tool bug for LPDDR4 devices
- added info and validation reports for Nanya devices