Seleccione una versión

Seleccione una versión

No se encontraron resultados. Borre su búsqueda y vuelva a intentarlo.

PROCESSOR-SDK-LINUX-K2G

Linux Processor SDK for K2Gx

Seleccione una versión
No se encontraron resultados. Borre su búsqueda y vuelva a intentarlo.
Última versión
Versión: 06.03.00.106
Fecha de publicación: 19/04/2020

K2G EVM Linux SDK (64-bit Binary)

Suma de comprobación SHA-256

Code Composer Studio IDE for Windows Host

Code Composer Studio IDE for Linux Host

Only used when creating an SD Card on Windows

Suma de comprobación SHA-256

Standalone ARM Toolchain - ARM GCC 8.3 2019.03 hard-float toolchain

K2G Linux SDK BSP Source Code

Suma de comprobación SHA-256

K2G Linux SDK prebuilt BSP binaries and root filesystem

Suma de comprobación SHA-256

K2G Linux SDK Arago source downloads

Suma de comprobación SHA-256

Quick Start Guide that was included in the EVM kit

Productos
SoC del procesador de señal digital (DSP) de radar y audio
66AK2G12 — DSP+Arm multinúcleo de alto rendimiento: 1x Arm, núcleos A15, 1x C66x DSP núcleo

Documentación

Instructions for creating an SD Card with Linux

Instructions for creating an SD Card with Windows

Link to Release Notes for Processor SDK Linux

Link to the online Software Developers Guide which has the latest content

Software Manifest of Components Inside the SDK

Información de la versión

Thank you for your interest in the K2G Software Development Kit (SDK). If you would like to install the full SDK on a Linux Host computer for development, you'll need the K2G Linux SDK Essentials below. If you would like to evaluate the SDK by running it on one of the below platforms and you prefer not to install the full SDK at this time, please see the K2G Linux SDK SD Card Creation section below.

More Information If you'd like more information on all of these choices, please refer to the Processor SDK Linux Getting Started Guide (GSG) below or the latest version here . For a complete overview of the SDK, please refer to the Processor SDK Linux Software Developer's Guide (SDG) below or the latest version here .