Performing grip detection by inductive touch using the LDC3114

This video covers how to use an inductive touch device like the LDC3114 to implement a grip detection solution on a handle.

00:05:43|07 Mar 2025

The LDC3114 is one of TI's inductive sensing devices that is capable of providing a high-resolution inductance measurement or button press outputs using an internal baseline tracking algorithm. In this video, we use the baseline tracking along with the digital button outputs of the device to determine when a user is gripping a handle.