SBOS716D May 2015 – January 2020 TMP107
PRODUCTION DATA.
The C/nA bit indicates whether the current communication is a command operation or address operation. The C/nA bit = 1 indicates a command operation. The codes for specific commands in the TMP107 are listed in Table 2. Codes other than those listed in Table 2 are reserved for factory use only.
The C/nA bit = 0 indicates an address operation. The five bits following the C/nA bit (A4 to A0) are the address bits of the device or devices that the host intends to communicate with in the chain, as shown in Figure 20.