SBOSA41A May 2023 – September 2023 TMP4718
PRODUCTION DATA
The ALERT pin of the device can be programmed into two different ALERT output modes. In the interrupt mode, the device will assert the ALERT pin if the temperature exceeds the limits set by the temperature limit registers. After the Alert Status is read and interrupt bits cleared, the ALERT pin is deasserted. In Comparator Mode, the device will assert the ALERT pin if the measured temperature exceeds the limits and clear when the temperature returns below the limits.