SLUSD49A September 2017 – January 2019 UCC256303
PRODUCTION DATA.
Refer to the PDF data sheet for device specific package drawings
During burst off period, power consumed by the high side gate driver from the HB pin must be drawn from CBOOT and will cause its voltage to decay. At the start of the next burst period there must be sufficient voltage remaining on CBOOT to power the high side gate driver until the conduction period of LO allows it to be replenished from CRVCC. The power consumed by the high side driver during this burst off period will therefore have a direct impact on the size and cost of capacitors that must be connected to CBOOT and RVCC.
Assume the system has a maximum burst off period of 10 ms.
Assume the bootstrap diode has a forward voltage drop of 1 V:
Assume the boot voltage to be always above 8 V to avoid UVLO fault. Then the maximum allowed voltage drop on boot capacitor is:
Boot capacitor can then be sized: