SLUSD49A September 2017 – January 2019 UCC256303
PRODUCTION DATA.
Refer to the PDF data sheet for device specific package drawings
Ln is the ratio between the magnetizing inductance and the resonant inductance.
Qe is the quality factor of the resonant tank.
In this equation, Re is the equivalent load resistance.
Selecting Ln and Qe values should result in an LLC gain curve, as shown below, that intersects with Mg(min) and Mg(max) traces. The peak gain of the resulting curve should be larger than Mg(max). Details of how to select Ln and Qe are not discussed here. They are available in the Application Note, UCC25630x Practical Design Guidelines and UCC256303 Design Calculator.
In this case, the selected Ln and Qe values are: