JAJSP50A May 2023 – September 2023 AMC131M03-Q1
PRODUCTION DATA
The STANDBY command places the device in a low-power standby mode. The command is latched by the device at the end of the frame. The device enters standby mode immediately after the command is latched. Set the DCDC_EN bit in the DCDC_CTRL register to 0b to disable the DC/DC converter before entering standby mode. See the Standby Mode section for more information. This command has no effect if the device is already in standby mode.