JAJSCB3E June 2016 – April 2019 BQ35100
PRODUCTION DATA.
The BQ35100 device only has one active power mode that is enabled through the GAUGE ENABLE (GE) pin. The power consumption of the BQ35100 device can change significantly based on host commands it receives and its default configuration, specifically with respect to data flash updates.
For information on how to configure the device to influence the average power consumption, see the Power Control section in the BQ35100 Technical Reference Manual (SLUUBH1).