JAJSHL4C March 2015 – June 2019 DLPC150
PRODUCTION DATA.
PIN | I/O(1) | DESCRIPTION | |||||||
---|---|---|---|---|---|---|---|---|---|
NAME | NO. | ||||||||
CONTROL AND INITIALIZATION | |||||||||
RESETZ | C11 | I6 | DLPC150 power-on reset (active low input) (hysteresis buffer). Self-configuration starts when a low-to-high transition is detected on RESETZ. All DLPC150 controller power and clocks must be stable before this reset is de-asserted. Connect to the reset output pin (RESETZ) of the DLPA2000 or DLPA2005 PMIC. Note that the following signals will be tri-stated while RESETZ is asserted:
SPI0_CLK, SPI0_DOUT, SPI0_CSZ0, SPI0_CSZ1, PMIC_SPI_CLK, PMIC_SPI_CSZ, PMIC_SPI_DIN, PMIC_SPI_DOUT, TRIG_OUT_1, TRIG_OUT_2, and GPIO[19:05] External pullups or downs (as appropriate) should be added to all tri-stated output signals listed (including bidirectional signals to be configured as outputs) to avoid floating DLPC150 controller outputs during reset if connected to devices on the PCB that can malfunction. For SPI, at a minimum, any chip selects connected to the devices should have a pullup. Unused bidirectional signals can be functionally configured as outputs to avoid floating DLPC150 controller inputs after RESETZ is set high. The following signals are forced to a logic low state while RESETZ is asserted and corresponding I/O power is applied: LED_SEL_0, LED_SEL_1 and DMD_DEN_ARSTZ No signals will be in their active state while RESETZ is asserted. Note that no I2C activity is permitted for a minimum of 500 ms after RESETZ (and PARKZ) are set high. |
||||||
PARKZ | C13 | I6 | DMD fast PARK control (active low Input) (hysteresis buffer). PARKZ must be set high to enable normal operation. PARKZ should be set high prior to releasing RESETZ (that is, prior to the low-to-high transition on the RESETZ input). PARKZ should be set low for a minimum of 40 µs before any power is removed from the DLPC150 such that the fast DMD PARK operation can be completed. Note for PARKZ, fast PARK control should only be used when loss of power is eminent and beyond the control of the host processor (for example, when the external power source has been disconnected or the battery has dropped below a minimum level). The longest lifetime of the DMD may not be achieved with the fast PARK operation. The longest lifetime is achieved with a normal PARK operation. Because of this, PARKZ is typically used in conjunction with a normal PARK request control input through PROJ_ON. The difference being that when the host sets PROJ_ON low, which connects to both DLPC150 and the DLPA200x PMIC chip, the DLPC150 takes much longer than 40 µs to park the mirrors. The DLPA200x holds on all power supplies, and keep RESETZ high, until the longer mirror parking has completed. This longer mirror parking time, of up to 20 ms, ensures the longest DMD lifetime and reliability.
The DLPA2000 or DLPA2005 monitors power to the DLPC150 and detects an eminent power loss condition and drives the PARKZ signal accordingly. Connect to the interrupt output pin of the DLPA2000 or DLPA2005 PMIC. |
||||||
PROJ_ON | G14 | B1 | Normal mirror parking request (active low): To be driven by the PROJ_ON output of the host. A logic low on this signal will cause the DLPC150 to PARK the DMD, but it will not power down the DMD (the DLPA2000 or DLPA2005 controls the power down). The minimum high time is 200 ms. The minimum low time is also 200 ms. | ||||||
HOST_IRQ(2) | N8 | O9 | Host interrupt (output)
This signal has two primary uses. The first use is to indicate when DLPC150 auto-initialization is in progress and most importantly when it completes. The second is to indicate when service is requested (that is an interrupt request). The DLPC150 tri-states this output during reset and requires an external pullup to drive this signal to its inactive state. |
||||||
IIC0_SCL | N10 | B7 | I2C slave (port 0) SCL A bidirectional, open-drain signal with input hysteresis that requires an external pullup. The slave I2C I/Os are 3.6-V tolerant (high-volt-input tolerant) and are powered by VCC_INTF (which can be 1.8, 2.5, or 3.3 V). External I2C pullups must be connected to an equal or higher supply voltage, up to a maximum of 3.6 V (a lower pullup supply voltage would not likely satisfy the VIH specification of the slave I2C input buffers). | ||||||
IIC0_SDA | N9 | B7 | I2C slave (port 0) SDA. A bidirectional, open-drain signal with input hysteresis that requires an external pullup. The slave I2C I/Os are 3.6-V tolerant (high-volt-input tolerant) and are powered by VCC_INTF (which can be 1.8, 2.5, or 3.3 V). External I2C pullups must be connected to an equal or higher supply voltage, up to a maximum of 3.6 V (a lower pullup supply voltage would not likely satisfy the VIH specification of the slave I2C input buffers). | ||||||
PARALLEL PORT INPUT DATA AND CONTROL | |||||||||
PCLK | P3 | I11 | Pixel clock(5) | ||||||
PDM_CVS_TE | N4 | B5 | Parallel data mask(3) | ||||||
VSYNC_WE | P1 | I11 | Vsync(4) | ||||||
HSYNC_CS | N5 | I11 | Hsync(4) | ||||||
DATAEN_CMD | P2 | I11 | Data valid active high framing signal.(4) DLPC150 also offers a manual data framing mode through a software command. Refer to the DLPC150 Programmer's Guide for more information on the manual data framing command. | ||||||
(TYPICAL RGB 888) | |||||||||
PDATA_0
PDATA_1 PDATA_2 PDATA_3 PDATA_4 PDATA_5 PDATA_6 PDATA_7 |
K2
K1 L2 L1 M2 M1 N2 N1 |
I11 | Blue
Blue Blue Blue Blue Blue Blue Blue |
||||||
(TYPICAL RGB 888) | |||||||||
PDATA_8
PDATA_9 PDATA_10 PDATA_11 PDATA_12 PDATA_13 PDATA_14 PDATA_15 |
R1
R2 R3 P4 R4 P5 R5 P6 |
I11 | Green
Green Green Green Green Green Green Green |
||||||
(TYPICAL RGB 888) | |||||||||
PDATA_16
PDATA_17 PDATA_18 PDATA_19 PDATA_20 PDATA_21 PDATA_22 PDATA_23 |
R6
P7 R7 P8 R8 P9 R9 P10 |
I11 | Red
Red Red Red Red Red Red Red |
||||||
DMD RESET AND BIAS CONTROL | |||||||||
DMD_DEN_ARSTZ | B1 | O2 | DMD driver enable (active high)/ DMD reset (active low). Assuming the corresponding I/O power is supplied, this signal will be driven low after the DMD is parked and before power is removed from the DMD. If the 1.8-V power to the DLPC150 is independent of the 1.8-V power to the DMD, then TI recommends a weak, external pulldown resistor to hold the signal low in the event DLPC150 power is inactive while DMD power is applied. | ||||||
DMD_LS_CLK | A1 | O3 | DMD, low speed interface clock | ||||||
DMD_LS_WDATA | A2 | O3 | DMD, low speed serial write data | ||||||
DMD_LS_RDATA | B2 | I6 | DMD, low speed serial read data | ||||||
DMD SUB-LVDS INTERFACE | |||||||||
DMD_HS_CLK_P
DMD_HS_CLK_N |
A7
B7 |
O4 | DMD high speed interface | ||||||
DMD_HS_WDATA_H_P
DMD_HS_WDATA_H_N DMD_HS_WDATA_G_P DMD_HS_WDATA_G_N DMD_HS_WDATA_F_P DMD_HS_WDATA_F_N DMD_HS_WDATA_E_P DMD_HS_WDATA_E_N DMD_HS_WDATA_D_P DMD_HS_WDATA_D_N DMD_HS_WDATA_C_P DMD_HS_WDATA_C_N DMD_HS_WDATA_B_P DMD_HS_WDATA_B_N DMD_HS_WDATA_A_P DMD_HS_WDATA_A_N |
A3
B3 A4 B4 A5 B5 A6 B6 A8 B8 A9 B9 A10 B10 A11 B11 |
O4 | DMD high speed interface lanes, write data bits: (The true numbering and application of the DMD_HS_DATA pins are software configuration dependent) | ||||||
SERIAL FLASH MEMORY INTERFACE | |||||||||
SPI0_CLK | A13 | O13 | Synchronous serial port 0, clock output. Connect to clock input pin of the serial Flash memory device. | ||||||
SPI0_CSZ0 | A14 | O13 | Synchronous serial port 0, chip select 0 output. Active low output. Connect to chip select pin of the serial Flash memory device.
TI recommends an external pullup resistor to avoid floating inputs to the external SPI device during DLPC150 controller reset assertion. |
||||||
SPI0_CSZ1 | C12 | O13 | Synchronous serial port 0, chip select 1 output. Active low output. Connect to chip select pin of a second serial Flash memory device.
TI recommends an external pullup resistor to avoid floating inputs to the external SPI device during DLPC150 controller reset assertion. |
||||||
SPI0_DIN | B12 | I12 | Synchronous serial port 0, receive data input. Connect to the data output of the serial Flash memory device. | ||||||
SPI0_DOUT | B13 | O13 | Synchronous serial port 0, transmit data output. Connect to the data input of the serial Flash memory device. | ||||||
DLPA2000 OR DLPA2005 PMIC INTERFACE | |||||||||
PMIC_SPI_CLK | C15 | B1 | Synchronous PMIC serial port, clock output. Connect to the clock input (SPI_CLK) of the DLPA2000 or DLPA2005 PMIC. | ||||||
PMIC_SPI_CSZ | D15 | B1 | Synchronous PMIC serial port, chip select output. Active low output. Connect to the chip select input (SPI_CSZ) of the DLPA2000 or DLPA2005 PMIC.
TI recommends an external pullup resistor to avoid floating inputs to the external SPI device during DLPC150 controller reset assertion. |
||||||
PMIC_SPI_DIN | C14 | B1 | Synchronous PMIC serial port, receive data input. Connect to the data output (SPI_DOUT) of the DLPA2000 or DLPA2005 PMIC. | ||||||
PMIC_SPI_DOUT | D14 | B1 | Synchronous PMIC serial port, receive data output. Connect to the data input (SPI_DIN) of the DLPA2000 or DLPA2005 PMIC. | ||||||
PMIC_CMP_IN | A12 | I6 | Successive approximation ADC comparator input. Assumes a successive approximation ADC is implemented with a WPC light sensor and/or a thermistor feeding one input of an external comparator and the other side of the comparator is driven from the DLPC150 controller’s CMP_PWM pin. Connect to the analog comparator output (CMP_OUT) of the DLPA2000 or DLPA2005 PMIC. If this function is not used, pulled-down to ground. | ||||||
PMIC_CMP_PWM | A15 | O1 | Successive approximation comparator pulse-duration modulation output. Supplies a PWM signal to drive the successive approximation ADC comparator used in WPC light-to-voltage sensor applications. Connect to the reference voltage input for analog comparator (PWM_IN) of the DLPA2000 or DLPA2005. If this function is not used, leave this pin unconnected. | ||||||
PMIC_LED_SEL_0 | B15 | O1 | LED enable select. Controlled by programmable DMD sequence | ||||||
LED_SEL(1:0) | Enabled LED Timing
DLPA2000 or DLPA2005 application 00 = None 01 = Red 10 = Green 11 = Blue |
||||||||
PMIC_LED_SEL_1 | B14 | O1 | These signals will be driven low when RESETZ is asserted and the corresponding I/O power is supplied. They will continue to be driven low throughout the auto-initialization process. A weak, external pulldown resistor is still recommended to ensure that the LEDs are disabled when I/O power is not applied. | ||||||
TRIGGER CONTROL | |||||||||
TRIG_IN_1 | N6 | I11 | Input Trigger mode 1. Active high input signal that display the next pattern in the pattern sequence. Pull-down this signal with an external resistor. | ||||||
TRIG_OUT_1 | L14 | B1 | Output Trigger mode 1. Active high output signal during pattern exposure | ||||||
TRIG_OUT_2 | E14 | B1 | Output Trigger mode 2. Active high output signal that indicates the first pattern in a sequence. | ||||||
GPIO PERIPHERAL INTERFACE | |||||||||
GPIO_19 | M15 | B1 | General purpose I/O 19 (hysteresis buffer). Options:
|
||||||
GPIO_18 | M14 | B1 | General purpose I/O 18 (hysteresis buffer). Options:
|
||||||
GPIO_17 | L15 | B1 | General purpose I/O 17 (hysteresis buffer). Options:
|
||||||
GPIO_15 | K15 | B1 | General purpose I/O 15 (hysteresis buffer). Options:
|
||||||
GPIO_14 | K14 | B1 | General purpose I/O 14 (hysteresis buffer). Option:
|
||||||
GPIO_13 | J15 | B1 | General purpose I/O 13 (hysteresis buffer). Options:
|
||||||
GPIO_12 | J14 | B1 | General purpose I/O 12 (hysteresis buffer). Option:
|
||||||
GPIO_11 | H15 | B1 | General purpose I/O 11 (hysteresis buffer). Options:
|
||||||
GPIO_10 | H14 | B1 | General Purpose I/O 10 (hysteresis buffer). Options:
|
||||||
GPIO_09 | G15 | B1 | General purpose I/O 09 (hysteresis buffer). Options:
|
||||||
GPIO_07 | F15 | B1 | General purpose I/O 07 (hysteresis buffer). Options:
|
||||||
GPIO_06 | F14 | B1 | General purpose I/O 06 (hysteresis buffer). Option:
|
||||||
GPIO_05 | E15 | B1 | General purpose I/O 05 (hysteresis buffer). Option:
|
||||||
CLOCK AND PLL SUPPORT | |||||||||
PLL_REFCLK_I | H1 | I11 | Reference clock crystal input. If an external oscillator is used in place of a crystal, then this pin serves as the oscillator input. | ||||||
PLL_REFCLK_O | J1 | O5 | Reference clock crystal return. If an external oscillator is used in place of a crystal, then leave this pin unconnected with no capacitive load. | ||||||
BOARD LEVEL TEST AND DEBUG | |||||||||
HWTEST_EN | C10 | I6 | Reserved Manufacturing test enable pin. For proper device operation, connect this signal directly to ground. | ||||||
Reserved | P12 | I6 | Reserved pin. For proper device operation, leave this pin unconnected. | ||||||
Reserved | P13 | I6 | Reserved pin. For proper device operation, leave this pin unconnected. | ||||||
Reserved | N13(6) | O1 | Reserved pin. For proper device operation, leave this pin unconnected. | ||||||
Reserved | N12(6) | O1 | Reserved pin. For proper device operation, leave this pin unconnected. | ||||||
Reserved | R10 | B8 | Reserved pin. For proper device operation, pull high to Vcc18 with external pullup resistor. | ||||||
Reserved | R11 | B8 | Reserved pin. For proper device operation, pull high to Vcc18 with external pullup resistor. | ||||||
Reserved | M13 | I6 | Reserved pin. For proper device operation, leave this pin unconnected. | ||||||
Reserved | N11 | I6 | Reserved pin. For proper device operation, leave this pin unconnected. | ||||||
Reserved | P11 | I6 | Reserved pin.
For proper device operation, this pin must be tied to ground, through an external 8-kΩ, or less, resistor. Failure to tie this pin low will cause startup and initialization problems. |
||||||
Reserved | E1 | Reserved pin. For proper device operation, leave this pin unconnected. | |||||||
Reserved | E2 | Reserved pin. For proper device operation, leave this pin unconnected. | |||||||
Reserved | F1 | Reserved pin. For proper device operation, leave this pin unconnected. | |||||||
Reserved | F2 | Reserved pin. For proper device operation, leave this pin unconnected. | |||||||
Reserved | F3 | Reserved pin. For proper device operation, leave this pin unconnected. | |||||||
Reserved | G1 | Reserved pin. For proper device operation, leave this pin unconnected. | |||||||
Reserved | G2 | Reserved pin. For proper device operation, leave this pin unconnected. | |||||||
Reserved | D1 | Reserved pin. For proper device operation, leave this pin unconnected. | |||||||
Reserved | D2 | Reserved pin. For proper device operation, leave this pin unconnected. | |||||||
Reserved | C1 | Reserved pin. For proper device operation, leave this pin unconnected. | |||||||
Reserved | C2 | Reserved pin. For proper device operation, leave this pin unconnected. | |||||||
TSTPT_0 | R12 | B1 | Reserved Test pin 0. For proper device operation, leave this pin unconnected (includes weak internal pulldown).Tri-stated while RESETZ is asserted low. Sampled as an input test mode selection control approximately 1.5 µs after de-assertion of RESETZ, and then driven as an output.
Note: An external pullup should not be applied to this pin to avoid putting the DLPC150 in a test mode. |
||||||
TSTPT_1 | R13 | B1 | Reserved Test pin 1. For proper device operation, leave this pin unconnected (includes weak internal pulldown). Tri-stated while RESETZ is asserted low. Sampled as an input test mode selection control approximately 1.5 µs after de-assertion of RESETZ and then driven as an output.
Note: An external pullup should not be applied to this pin to avoid putting the DLPC150 in a test mode. |
||||||
TSTPT_2 | R14 | B1 | Reserved Test pin 2. For proper device operation, leave this pin unconnected (includes weak internal pulldown). Tri-stated while RESETZ is asserted low. Sampled as an input test mode selection control approximately 1.5 µs after de-assertion of RESETZ and then driven as an output.
Note: An external pullup should not be applied to this pin to avoid putting the DLPC150 in a test mode. |
||||||
TSTPT_3 | R15 | B1 | Reserved Test pin 3. For proper device operation, leave this pin unconnected (includes weak internal pulldown).Tri-stated while RESETZ is asserted low. Sampled as an input test mode selection control approximately 1.5 µs after de-assertion of RESETZ and then driven as an output. | ||||||
TSTPT_4 | P14 | B1 | Reserved Test pin 4. For proper device operation, leave this pin unconnected (includes weak internal pulldown).Tri-stated while RESETZ is asserted low. Sampled as an input test mode selection control approximately 1.5 µs after de-assertion of RESETZ and then driven as an output. | ||||||
TSTPT_5 | P15 | B1 | Reserved Test pin 5. For proper device operation, leave this pin unconnected (includes weak internal pulldown). Tri-stated while RESETZ is asserted low. Sampled as an input test mode selection control approximately 1.5 µs after de-assertion of RESETZ and then driven as an output. | ||||||
TSTPT_6 | N14 | B1 | Reserved Test pin 6. For proper device operation, leave this pin unconnected (includes weak internal pulldown). Tri-stated while RESETZ is asserted low. Sampled as an input test mode selection control approximately 1.5 µs after de-assertion of RESETZ and then driven as an output. | ||||||
TSTPT_7 | N15 | B1 | Reserved Test pin 7. For proper device operation, leave this pin unconnected (includes weak internal pulldown). Tri-stated while RESETZ is asserted low. Sampled as an input test mode selection control approximately 1.5 µs after de-assertion of RESETZ and then driven as an output. | ||||||
POWER AND GROUND | |||||||||
VDD | C5, D5, D7, D12, J4, J12, K3, L4, L12, M6, M9, D9, D13, F13, H13, L13, M10, D3, E3 | PWR | Core power 1.1 V (main 1.1 V) | ||||||
VDDLP12 | C3 | PWR | Core power 1.1 V | ||||||
VSS | C4, D6, D8, D10, E4, E13, F4, G4, G12, H4, H12, J3, J13, K4, K12, L3, M4, M5, M8, M12, G13, C6, C8, F6, F7, F8, F9, F10, G6, G7, G8, G9, G10, H6, H7, H8, H9, H10, J6, J7, J8, J9, J10, K6, K7, K8, K9, K10 | GND | Core ground (eDRAM, I/O ground, thermal ground) | ||||||
VCC18 | C7, C9, D4, E12, F12, K13, M11 | PWR | All 1.8-V I/O power:
(1.8-V power supply for all I/O other than the host or parallel interface and the SPI flash interface. This includes RESETZ, PARKZ LED_SEL, CMP, GPIO, IIC1, TSTPT, and JTAG pins) |
||||||
VCC_INTF | M3, M7, N3, N7 | PWR | Host or parallel interface I/O power: 1.8 to 3.3 V (Includes IIC0, PDATA, video syncs, and HOST_IRQ pins) | ||||||
VCC_FLSH | D11 | PWR | Flash interface I/O power:1.8 to 3.3 V
(Dedicated SPI0 power pin) |
||||||
VDD_PLLM | H2 | PWR | MCG PLL 1.1-V power | ||||||
VSS_PLLM | G3 | RTN | MCG PLL return | ||||||
VDD_PLLD | J2 | PWR | DCG PLL 1.1-V power | ||||||
VSS_PLLD | H3 | RTN | DCG PLL return |