JAJSIW8 April 2020 LM5181-Q1
PRODUCTION DATA.
To minimize output voltage regulation error, the LM5181-Q1 senses the reflected secondary voltage when the secondary current reaches zero. The feedback (FB) resistor, which is connected between SW and FB as shown in Figure 17, is determined using Equation 8.
where