JAJSDN3F December 2016 – April 2024 TDP158
PRODUCTION DATA
The TDP158 has the ability to perform as a DisplayPort redriver under the right conditions. The TDP158 is put into this mode by setting reg09h[5] to 1. The device is now programmable through I2C only. As the transmitter is a DC coupled transmitter supporting TMDS some external circuits are required to level shift the signal to an AC-coupled DisplayPort signal, see Figure 8-6. Note that the AUX lines bypass the TDP158. To set the device up correctly during link training, the TDP158 must be programmed using I2C. When this bit is set, the TDP158 does the following:
For the system implementer to configure the TDP158 output to the properly requested levels during link training, the following registers are used.
Power down states while in DP-Mode are implemented the same as if in normal operation. See Section 5.7 for the outputs based upon the VSADJ 6kΩ VSADJ resistor.