JAJSDF4A May 2017 – May 2019 TMP116
PRODUCTION DATA.
When in shutdown mode, a single conversion can be performed by writing 11 to MOD bits in the configuration register, referred to as a one-shot conversion. After completing a one-shot conversion, the device returns to the low-power shutdown mode. A one-shot conversion cycle only consists of active conversion time and no standby period unlike CC mode. Thus, the duration of a one-shot conversion is only affected by the settings in the AVG bits. Figure 21 shows a timing diagram for this mode with an AVG setting of 00 and Figure 22 shows a timing diagram for this mode with an AVG setting of 01. At the end of a one-shot conversion, the Data_Ready flag in the configuration register is set. The Data_Ready flag is cleared by read of the configuration register or temperature result register. The state of the Data_Ready flag can also be monitored on the ALERT pin by setting the DR/nAlert_EN bit in the configuration register.