JAJSCO1A November 2016 – September 2021 TPS3851
PRODUCTION DATA
WDI is the watchdog timer input that controls the WDO output. The WDI input is triggered by the falling edge of the input signal. To ensure proper functionality of the watchdog timer, always issue the WDI pulse before tWD(min). If the pulse is issued in this region, then WDO remains unasserted. Otherwise, the device asserts WDO, putting the WDO pin into a low-impedance state.
The watchdog input (WDI) is a digital pin. To
ensure there is no increase in IDD, drive the WDI pin to either VDD or
GND at all times. Putting the pin to an intermediate voltage can cause an increase
in supply current (IDD) because of the architecture of the digital logic
gates. When RESET is asserted, the watchdog is disabled and all
signals input to WDI are ignored. When RESET is no longer
asserted, the device resumes normal operation and no longer ignores the signal on
WDI. If the watchdog is disabled, drive the WDI pin to either VDD or GND.
Figure 7-2 shows the valid region for a WDI pulse to be issued to prevent
WDO from being triggered and pulled low.