JAJSSS6 January 2024 TPS7H3014-SP
ADVANCE INFORMATION
If active, the REG_TMR will monitor the time a VOUTx takes to cross the VONx voltage once the ENx signal is forced high. In the case the REG_TMR is expired and VOUTx has not crossed the VONx voltage, a reverse sequence down from the previously sequenced rail will be started as described in the State Machine State Machine State Machine section. Figure 7-8 shows the REG_TMR active during sequence up, from the time ENx is forced high (VOUTx starts rising). In this case, VOUTx always crosses VON before the timer is expired. The REG_TMR resistor can be selected using Equation 16. Figure 7-10 shows the linear trend between the REG_TMR resistor and the regulation time allowed for the rail to be in regulation (VOUTx > VONx).
Table 7-2 shows typical resistor values for different allowed regulation times.
Allowed Regulation Time (ms) | RREG_TMR (kΩ) |
---|---|
0.264 | 10.5 |
12.4 | 619 |
23.63 | 1180 |