DLPU113A December 2021 – April 2022 DLP2021-Q1
The first step in running the GUI requires the user to establish connection to the FTDI cable. The GUI will attempt to automatically connect to the FTDI cable at start-up. To manually connect the FTDI cable, navigate to the Connection page. With the FTDI cable selected from the drop-down interface list, click the Connect button. Note, the Connection settings must be a clock rate of 5 MHz and timeout of 500 ms. When using the Cheetah™ interface, the clock rate can be increased to 16 MHz in SPI Mode 0 and MSB first bit order.
The FTDI cable must be disconnected/released from DLP Composer if DLP Composer was previously used to flash program the EVM. The FTDI cable cannot be shared simultaneously between DLP Composer and DLP Control Program.