The DLPLCRC910EVM is ready to use after assembling
with a supported DMD EVM and a front end board such as the AMD Xilinx VC-707 EVM.
Steps 1 through 6 show how to power, display an image, and connect the EVM to a
PC.
- Before connecting the AMD Xilinx
VC-707 board program the configuration PROM per the instructions in AMD Xilinx VC-707 Configuration PROM
ProgrammingUSB Firmware Programming.
- Connect a 12-V DC power supply to the power supply connector J15 in Figure 3-4.
- LED — D4 illuminates if power is present at J15.
- Power on the AMD Xilinx VC-707
board.
Note: Allow sufficient time for the VC-707 board
to configure (10 seconds is suggested).
- Turn on SW3 [DMD Park
(PWR_FLOAT)].
- Turn on SW4 [Power Enable].
- LED — D7 illuminates indicating that the PROM has configured
the DLPC910.
- LED — D2 briefly illuminates
indicating calibration is in progress and goes out when complete.
- LED — D1 flashes (heartbeat) to
indicating that the DLPC910 is running.
Note: A DMD EVM
board and a properly configured AMD Xilinx VC-707 board must be present for
the DLPC910 to initialize.
- Connect a USB cable from a PC to connector J1 on the DLPLCRC910EVM, as seen in
Figure 3-4. The first time the cable is connected on a PC, the DLPLCRC910EVM enumerates.
The required drivers are installed as part of the DLPLCRC910EVM GUI
installation.
- The DLPLCRC910EVM can be controlled with the GUI software available for
download from the DLPLCRC910EVM Tool Folder.