The SPI Flash can be programmed over the
JTAG interface using a USB-JTAG cable supported by AMD Xilinx ISE Impact Tool. The procedure
has been tested with ISE Impact Tool version 14.1 (32 bit) with a Digilent® JTAG-HS2 programmer.
Note:
Use of other ISE Impact Tool versions
have resulted in the SPI Flash programming incorrectly.
Please contact AMD Xilinx for support
with other programming platform cables.
The DLPC910 SPI Flash MCS file to use in this procedure is found here: DLPR910
- Open up the Impact application.
- Power on the DLPLCRC910EVM and connect
the JTAG-HS2 programming cable to J17 DLPLCRC910EVM Connectors (Top View) and then to the PC that you have the IMPACT Tool installed on.
Note: Do not connect the AMD Xilinx VC-707 board.
- Once the program is open, select either to start a new project
- Select Configure device using
Boundary-Scan (JTAG) which initializes the JTAG chain.
- The IMPACT Tool prompts to assign a
SPI/BPI PROM to the device. Select Yes to attach a SPI PROM to the Controller.
Note: Only .mcs files are able to be assigned to the SPI PROM; anything
else results in an error.
- Select SPI PROM and S25FL032P with a data width of 1 and press
OK.
- Select Yes to ignore the data width warning.
- To program the device through IMPACT Tool, right-click on the FLASH and click
Program. User can also select Program under Impact Processes on the
bottom left of the IMPACT Tool.
- The controller programs and reports Program Succeeded in the IMPACT Tool.
- Power down the DLPLCRC910EVM and remove the JTAG-HS2 programmer.