JAJSIC0J November 2009 – July 2021 TUSB1210
PRODUCTION DATA
In addition to the differential receiver, there is a single-ended receiver (SE–, SE+) for each of the two data lines D+/–. The main purpose of the single-ended receivers is to qualify the D+ and D– signals in the full-speed/low-speed modes of operation. See Section 6.8.