SBAU440 April   2024

 

  1.   1
  2.   Description
  3.   Get Started
  4.   Features
  5.   Applications
  6.   6
  7. 1Evaluation Module Overview
    1. 1.1 Introduction
    2. 1.2 Kit Contents
    3. 1.3 Specification
    4. 1.4 Device Information
  8. 2Hardware
    1. 2.1 ADS9219EVM Quick Start Guide
    2. 2.2 Analog Interface
      1. 2.2.1 High-bandwidth, Fully-Differential Circuit: THS4541
      2. 2.2.2 Voltage Reference
    3. 2.3 Power Supplies
      1. 2.3.1 USB Power and When to Power the Board Externally
  9. 3Software
    1. 3.1 Digital Interface and Clock Inputs
      1. 3.1.1 Digital Interface Connections
      2. 3.1.2 Clock Select
    2. 3.2 ADS9219EVM Software Reference
      1. 3.2.1 ADS9219EVM-GUI Software Installation
      2. 3.2.2 USB Driver Installation
      3. 3.2.3 Using the CONFIG Tab
      4. 3.2.4 Using the Capture Tab
      5. 3.2.5 Using the INL/DNL Tool
      6. 3.2.6 Using the Histogram Tab
  10. 4Hardware Design Files
    1. 4.1 Schematics
    2. 4.2 PCB Layout
    3. 4.3 Bill of Materials (BOM)
  11. 5Additional Information
    1. 5.1 Trademarks
  12. 6Related Documentation

ADS9219EVM-GUI Software Installation

This section details the installation and operation of the ADS9219EVM software graphical user interfaces (GUI). These software require the TSWDC155EVM (sold separately) controller to operate. The first step to installing the software (as shown in Figure 4-3) is to download the latest version of the EVM GUI installer as per Table 4-2.

Table 3-2 EVM GUI Installer
EVMSoftware Download Link
ADS9219EVMADS9219EVM-GUI

Accept all the license agreements and choose the destination location, project directory, and start menu. Typically, the default values work, but these values can be customized as needed based on the user's requirements. Next, the installer prompts the user to create a desktop icon and summarize the installation plan. Clicking Install begins copying software onto the computer. This process takes a few minutes. At completion, the user can launch a readme text file and the application. Figure 4-3 and Figure 4-4 show these steps.

Note: The GUI installer and GUI buttons can differ slightly depending on which specific GUI is being installed.
GUID-20240118-SS0I-ZCHC-FG4R-7XN8XJJP7JJV-low.svgFigure 3-3 Software Installation - Part 1
GUID-20240118-SS0I-VLW8-JT1G-TDXX8RCHSKM9-low.svgFigure 3-4 Software Installation - Part 2