The Limit configuration tab allows the user to set the values for the following warning limit registers:
- OUT_OC_WARN_LIMIT Register
- VIN_OV_WARN_LIMIT Register
- VIN_UV_WARN_LIMIT Register
- POUT_OP_WARN_LIMIT Register
The user is able to write and read these registers in the Device Configuration Tab as shown in
Figure 4-10. Refer to data sheet
Standard PMBus Commands section for register descriptions.