SLUAAM4 December 2023 BQ76905 , BQ76907
Table 3-9 shows how to read the BQ7690x device number. The device number can be read by first writing the subcommand number 0x0001 (little endian) to the command address 0x3E. This is followed by reading from the data buffer at address 0x40. In Figure 2-1, the device number returned is 0x7605 (which represents BQ76905).
Command | Name | Data | Units | Type | Description |
---|---|---|---|---|---|
0x0001 | DEVICE_NUMBER | Device Number | Hex | U2 | Reports the device number that identifies the product. The data is returned in little-endian format |